Issue:
Is there a Ramp available for Standard-Offer NetShelter SX cabinets?
Product Line:
NetShelter SX Cabinets
Environment:
All standard offer and serial ranges
Cause:
A customer wants to purchase a Ramp for a Standard-Offer NetShelter SX cabinet
Resolution:
There is no ramp included nor sellable for the NetShelter SX standard offers. Ramps are available in the NetShelter SX that comes with Shock Packaging. See sample diagram in the NetShelter SX w/ Shock Packaging Unpacking Instructions.
By design, the safest way to move the cabinet is by using a crane and the 4 holes in the top of the cabinet as is noted on the lower part of page 6 of the Installation, and Customization Manual .
For NetShelter with Shock Packaging / Shock Pallet, there is a sellable and reusable ramp AR9000RAMP.
Should there be any further concerns, please contact our Customer Care Center at https://www.apc.com/us/en/support/
發佈於:施耐德電機Taiwan