搜尋常見問題
Why can't I downgrade the BMENOC0301 or BMENOC0311?
This is due to a new NAND Flash hardware component introduced in Product Version (PV) 27 and greater.
If you have a BMENOC0301 or BMENOC0311 that is PV27 or greater, the lowest acceptable firmware level is v2.19.The downgrade procedure will fail if you attempt to downgrade the firmware below v2.19 with a PV27 or greater.
For more information on BMENOC0301 and BMENOC0311, please visit SE.com.
If you have a BMENOC0301 or BMENOC0311 that is PV27 or greater, the lowest acceptable firmware level is v2.19.The downgrade procedure will fail if you attempt to downgrade the firmware below v2.19 with a PV27 or greater.
For more information on BMENOC0301 and BMENOC0311, please visit SE.com.
發佈於:施耐德電機Taiwan
探索更多
產品:
探索更多
產品: