Issue:
Default IP address of a Premium PLC or ETY Ethernet module
Product Line:
Premium PLC
Resolution:
The ETY port on the processor or ETY module has a default IP address which is derived from the last 2 octets of the MAC address. The first 2 octets are fixed at 85.16.x.x ; where x.x is the last 2 octets of the MAC address. For example, If the MAC address is 00.80.F4.02.EA.6A then the IP address will be 85.16.234.106
Default IP address of a Premium PLC or ETY Ethernet module
Product Line:
Premium PLC
Resolution:
The ETY port on the processor or ETY module has a default IP address which is derived from the last 2 octets of the MAC address. The first 2 octets are fixed at 85.16.x.x ; where x.x is the last 2 octets of the MAC address. For example, If the MAC address is 00.80.F4.02.EA.6A then the IP address will be 85.16.234.106
EA Hex = 234 Decimal
6A Hex = 106 Decimal
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Опубліковано для:Schneider Electric Україна