Issue:
MultiDrive link error on the ATV930 Drives?
Product Line:
ATV930
Environment:
All
Cause:
MultiDrive link error can be triggered due to communication interruption between Server and Client drive. It can also be triggered if Multi Drive link function has detected an inconsistency in the system configuration.
Resolution:
Check the communication network.
Check the configuration of the multi-drive link function.
Check the firmware and make sure it is consistent on both drives.
Опубліковано для:Schneider Electric Україна