What is the power consumption of the fans in the NetShelter CX?
Issue:
There's a needs to know how much power is consumed by the NetShelter CX fans.

Product Line:
NetShelter CX

Environment:

All versions and serial ranges.

Cause:
It may be important to calculate total power consumption

Resolution:

NetShelter CX Mini = 30W
NetShelter CX/CX2 18U = 34W
NetShelter CX/CX2 24U = 68W
NetShelter CX/CX2 38U = 101W

Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: