Issue
What values should I expect to see, when using the 140ARI0300 to read Raw Resistance?
Product Line
Modicon Quantum
Environment
140ARI0300
Resolution
The data counts are 0-32767 counts converting for which ever range is selected (0-766.66 Ohms or 0-4000 Ohms). I.E. If configuring the range for the channel to 0-766.66 Ohms then 766.66 Ohms = 32767 counts (approx. 42.7 counts per Ohm.)
Опубліковано для:Schneider Electric Україна