With the IE (Indice Evolution) and the following table you can know the SV version inside
SV1.0 IE 19
SV1.1 IE 20
SV1.2 IE 21
SV1.3 IE 22
To show the IE version in connected mode on the module TSXCCY1128, typed : CTRL, SHIFT, F11 .
IE will appear near the SV.
Legacy KB System (APS) Data: RESL192736 V1.0, Originally authored by JeCa on 09/12/2008, Last Edited by JeCa on 09/12/2008
Related ranges: Modicon Premium
Опубліковано для:Schneider Electric Україна