Пошук серед найпопулярніших питань
What is the required CT wake-up percentage for the Energy Meter?
Issue:
Customer wants to know what is the minimum required percentage required for excitation on the Energy Meter.
Product Line:
EMB1010, EMB1021, EMB1032, EMB2010, EMB2021, EMB2032, EMB2043, EMB2083, EMB3010, EMB3010, EMB3021, EMB3032, EMB3043, EMB3083, EMB3084, EMB3164
Environment:
CT excitation
Cause:
CT's require a minimum excitation percentage.
Resolution:
According to Veris, a minimum of 2% is required. |