VISTA - How To Use A Custom Alarm Sound

Goals and Symptoms

VISTA - How To Use A Custom Alarm Sound

Causes and Fixes

If your computer is equipped with a sound card, you can replace the default alarm sound with a custom sound. Save the sound file you want to use as ''alarm.wav'' and store it in the ..\\System\\bin\\ETC directory.

Note: This information is also in ION Enterprise On-Line Help.

Original article#9353, SWKB-0522


Legacy KB System (APS) Data: RESL182674 V1.0, Originally authored by DaMi on 03/14/2007, Last Edited by DaMi on 03/14/2007
Related ranges: ION Enterprise

Schneider Electric Україна