Title
Can ION8300/ION8400/ION8500 Templates Be Uploaded to ION8600 or ION8650 meters?
Issue
When attempting to upload a meter template (.dcf) to an ION 8xxx meter, ION Setup will give an error if the meter template is incompatible with the destination meter.
Product Line
ION 8300
ION 8400
ION 8500
ION 8600
ION 8650
Environment
ION Setup
Cause
Due to feature differences among the different meters, only certain templates can be uploaded to certain meters.
Resolution
The following table shows the template compatibility between the different 8xxx meters.
8300 | 8400 | 8500 | 8600C | 8600B | 8600A | 8650C | 8650B | 8650A | |
ION 8300 framework will upload to | X | X | X | X | X | X | X | X | X |
ION 8400 framework will upload to | X | X | X | X | X | X | |||
ION 8500 framework will upload to | X | X | X | ||||||
ION 8600C framework will upload to | X | X | X | X | X | X | |||
ION 8600B framework will upload to | X | X | X | X | |||||
ION 8600A framework will upload to | X | X | |||||||
ION 8650C framework will upload to | X | X | X | ||||||
ION 8650B framework will upload to | X | X | |||||||
ION 8650A framework will upload to | X |
For example, an 8400 meter template will upload to the 8400, 8500, 8600B and 8600A meters. The 8400 will only accept templates from 8300 and 8400 meters.
Legacy KB System (APS) Data: RESL202158 V1.0, Originally authored by MiNe on 05/01/2010, Last Edited by MiNe on 05/01/2010
Related ranges: ION8600, ION8500, ION8400, ION8300
Опубліковано для:Schneider Electric Україна