Пошук серед найпопулярніших питань
Does Vijeo Designer support USB Mouse or Keyboard on the Magelis terminals?
Issue:
Does Vijeo Designer support USB Mouse or Keyboard on the Magelis terminals?
Product Line:
Magelis HMI programmed with Vijeo Designer V4.6 or higher (XBTGT, XBTGK, XBTGH, HMISTO, HMISTU, HMIGTO, HMIGTU, HMIGK, iPC)
Resolution:
Yes, Vijeo Designer V4.6 or higher supports USB Mouse or Keyboard on the Magelis terminals.
Опубліковано для:Schneider Electric Украина
Досліджуйте більше
Серія:
Досліджуйте більше
Серія: