Fundamental phasor readings unavailable in Firmware 16.007 of the Series 2000 Circuit Monitor (CM2000) when metering a Single Phase System.
Issue
Need to read the fundamental phasor readings from the CM2000

Product Line
CM2000

Environment
CM2000 with Firmware 16.007 or lower

Cause
There were no fundamental phasor readings on the CM2000 for firmware 16.007 and lower

Resolution
Upgrade to the latest firmware for the CM2000.
Firmware Files are located HERE
DLF3000 Utility is required to install the firmware. That utility can be found HERE

Schneider Electric Україна