Issue
The way that the 1120 command works changed in firmware version 10.204.
Product Line
CM3000
CM4000
Environment
Register Commands
Cause
The 1120 command in the CM4000 has historically cleared all memory. This command would clear all configuration registers including basic setup and communications parameters. The command would also clear all data log and alarm setup and all data log data.
This command has been modified and now requires the use of a parameter with the command to clear selected segments of the meter or to clear everything like the original command. This new command is implemented in the CM4000 in firmware versions beginning with 10.204. The following table provides a list of the parameters to clear selected segments of the meters memory.
Resolution
To issue commands using the command interface, follow these general steps:
- Write the related parameter(s) to the command parameter registers 8001 through 8015.
- Write the command code to the command interface register 8000.
Command | Parameters | Notes |
1120 | (8001) Bitmap of systems to reset | Restart System – Hard Reset with Memory Clear Bitmap of systems to reset: Bit 00 = Utility Registers Bit 01 = Reserved Bit 02 = CMPL Bit 03 = Config Display Bit 04 = Commands Bit 05 = Files Bit 06 = Alarms Bit 07 = I/O Points Bit 08 = Config Meter Bit 09 = Administrative Ctl Parameter value of 9999 causes meter to reset all registers to meter defaults and format the disk-on-chip. |
Parameter | Description |
Bit 00 = Utility Registers | Clear all utility register (15,800 - 15,999). |
Bit 01 = Reserved | |
Bit 02 = CMPL | Clears all custom Programs created in the meter. |
Bit 03 = Config Display | Clears all custom Displays created in the meter. |
Bit 04 = Commands | Clears all command interface registers. |
Bit 05 = Files | Clears all data log files (data and configuration). |
Bit 06 = Alarms | Clears all alarm configuration parameters. |
Bit 07 = I/O Points | Clears all I/O point configuration and assignments. |
Bit 08 = Config Meter | Clears all metering setup including PT and CT ratios. |
Bit 09 = Administrative Ctl | Clears all user account created in the meter. |
9999 = Clear All | Clears all memory in the meter (including comms). |
*NOTE: The 1120 command is disabled when revenue security is active.
*Reference CM3000 Register List Commands Page (Page 314).
*Reference CM4000 Register List Commands Page (Page 359).
Опубліковано для:Schneider Electric Україна