Release Notice
The purpose of this Resolution is to illustrate how to perform a backup and restore of the MBX driver configuration.
Goals and Symptoms
To create a backup file to be used during a restore, follow these steps listed below
Causes and Fixes
1) Launch the Schneider Electric MBX Driver Suite group
2) Select MBX Device Drivers3) Select the Diagnostics Tab
4) Select Backup or Restore
5) This will create a Backup file (Ex: C:\MBX.bak)
6) Example basic backup file…..
..
Опубліковано для:Schneider Electric Україна