Can I connect my VW3A1101 keypad directly to my PC to download / upload drive configuration files?

Issue:
Download/upload drive configuration files by connecting my VW3A1101 keypad directly to my PC.

Product Line:
VW3A1101 graphic HMI.

Environment:
All firmware revisions, all serial numbers

Cause:
Customer transferred files from several drives onto one keypad and now needs to copy them to their PC.

Resolution:
No, it is not possible to transfer files from the VW3A1101 keypad directly to a PC.  The keypad is used to store a backup copy of the program for transfer back into the same drive.  In order to copy the program from the drive in a format that can be easily transferred to a PC, either connect your PC directly to the drives Modbus RTU port via the RS232 to RS485 converter cable (TCSMCNAM3M002P) and use SoMove software to download the parameter, or use a multiloader handheld device.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Schneider Electric Україна

Досліджуйте більше
Серія:
Категорія:
Досліджуйте більше
Серія:
Категорія: