What is the part number for the Modbus Interface Module (IFM)
Issue
Part number for the Modbus Interface Module (IFM) to communicate with Compact NSX breakers

Product Line
Powerpact H, J & L breakers with Advanced Trip Units

Environment
Schneider Electric Catalog Number

Cause
Customers can not order the module without the part number

Resolution
The IFM catalog number is LV434000.  Previously the catalog number for the IFM was STRV00210 in North America or TRV00210 in the rest of the world.

Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: