Issue
Transferring authorization from computer to disk returns 'COMPNO NOT FOUND' error.
Product Line
ProWORX 32
Environment
Windows XP Professional, ProWORX 32
Resolution
If you try to transfer the authorization using the option ' transfer authorization from computer to disk', the ' 'COMPNO NOT FOUND' error could get returned.
The error can be ignored. If you click on OK and then click on Next, it will show that the authorization is already moved to the disk.
Transferring authorization from computer to disk returns 'COMPNO NOT FOUND' error.
Product Line
ProWORX 32
Environment
Windows XP Professional, ProWORX 32
Resolution
If you try to transfer the authorization using the option ' transfer authorization from computer to disk', the ' 'COMPNO NOT FOUND' error could get returned.
The error can be ignored. If you click on OK and then click on Next, it will show that the authorization is already moved to the disk.
- Click on 'NO'.
- Click on Cancel.
- Restart ProWORX 32.
Опубліковано для:Schneider Electric Україна