OFS v3.5 installs an older version of the 'Schneider Electric Software Update' tool.

Issue
OFS installs an older version of the 'Schneider Electric Software Update' tool.

Product Line
OPC Factory Server (OFS)

Environment
OFS version 3.5

Resolution
If you install an update to OFS, it will uninstall the newer version of the Schneider Electric Software Update tool
and replace it with an older version.

This is issue will no longer occur on future versions of OFS.  The SESU will be removed as part of the install
for OFS.  SESU currently does not monitor the SESU server for any OFS updates.  The SESU server is not
configured for OFS updates.  Currently installed versions of SESU by the OFS installation will never receive
an update notification.  It is for these reasons that Marketing has decided to remove the SESU from future
versions of OFS.

Schneider Electric Украина

Досліджуйте більше
Серія:
Modicon M580
Досліджуйте більше
Серія:
Modicon M580