Is there an EcoStruxure Web Services (EWS) reference client that can be installed to determine the data available from an EWS Server?
Issue:
Customer is not getting good data from their EWS client and would like to use an independent tool for troubleshooting

Product Line:
Struxureware Power Monitoring Expert 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Scada Expert 7.40
Power Scada Expert 8.x

Environment:
EWS Troubleshooting

Cause:
An EWS Reference Client is required for additional troubleshooting when EWS tags are not being pulled in correctly.

Resolution:

An EWS client that can be installed to test a PME/PSE EWS Server is attached. The attached document provides information on how to install the client and configure it for communication.

Schneider Electric Україна

Вкладення
EWSclientSetup.exe [3.03 MB]
EWS Reference Client Setup.docx [743.71 KB]
Досліджуйте більше
Продукт:
Статті, які можуть бути корисними
Досліджуйте більше
Продукт: