What is the temperature class of insulation for a Trihal Cast Resin Dry Type Transformers ?
The temperature class of insulation for a Trihal Cast Resin Dry Type Transformers is Class F  in accordance with IEC 60085 "Thermal evaluation and designation".

Schneider Electric Україна