ATV312- needs to run the drive without a motor connected

Article available in these languages: Spanish

Issue:
Programming the ATV312 to run without the motor connected.

Product Line:
ATV312 drives

Environment:
Run the drive without a motor connected

Cause:
ATV312- needs to run the drive without a motor connected

Resolution:
Suggested to go to FLT menu: set OPL to no.
Then can run the drive open circuit.



Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: