Issue:
Will the BMXP342020 or BMXNOE0110 communicate over Ethernet/IP?
Product Line:
M340, BMXNOE, BMXNOC, EIP, Modbus/TCP, MB/TCP
Resolution:
No, both P342020 and the BMXNOE support only Modbus/TCP. To get Ethernet/IP the BMXNOC module is required.
Will the BMXP342020 or BMXNOE0110 communicate over Ethernet/IP?
Product Line:
M340, BMXNOE, BMXNOC, EIP, Modbus/TCP, MB/TCP
Resolution:
No, both P342020 and the BMXNOE support only Modbus/TCP. To get Ethernet/IP the BMXNOC module is required.
Опубліковано для:Schneider Electric Україна