How can we have diagnostic information for TMC2xxx additional cartridge analog I/O module within a TM221Cxxx PLC SoMachine/Machine Expert - Basic application program ?
Within TM221Cxxx PLC and SoMachine/Machine Expert - Basic, we have the possibility to add 1 or 2 optional cartridges (depending on the TM221Cxxx PLC reference). Such cartridge provides 2 analog inputs or outputs channels as extension for the M221 PLC local I/Os.

For each channel, it exists a dedicated system word object available for diagnostic .
It’s  %IWS.0.i  for an analog input channel
It’s %QWS.0.i  for an analog output channel

With i defined by this way:
i=100  for  the 1st channel of the cartridge located 1st slot
i=101  for  the 2nd channel of the cartridge located  1st slot
i=200  for  the 1st channel of the cartridge located 2nd slot
i=201  for  the 2nd channel of the cartridge located 2nd slot

The definition of the code status/diagnostic value is as below:

For %IWS word content definition
0Normal
1Data conversion in progress
2Initialization in progress
3Input operation setting error or module without input
4not used
5High limit  reached
6Low limit reached
7Non-volatile memory error

For %QWS word content definition
0Normal state
1not used
2Initialization in progress( after power on)
3Output operation setting error or module without output
4not used
5not used
6not used
7Non-volatile memory error

Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: