When do the heatsink fans run on the ATV61 / ATV71 series drives?
Issue:
When do the heatsink fans run on the ATV61 / ATV71 series drives?

Product Line:
Altivar 61 and Altivar 71 series drives

Environment:
All models, All serial numbers.

Cause:
Information not available in current literature.

Resolution:
Heat sink fan operation differs depending on the frame size of the drive:
- for size 2 to 5B drives, fans start when the drive thermal state reaches a temperature level --> THD parameter = 70%.  The fans turns off when drive thermal is less than 60%
- for size 6 to 8 drives and 690V range drives, the fans run when the run command is given or when the drive thermal is greater than or equal to 70% and turns off when the drive thermal is less than 60% and runs for 1 minute after the run command is removed.
- for size 9 to 15 drives and 690V range drives, the fans run when the run command is given or when the drive thermal is greater than or equal to 70% and turns off when the drive thermal is less than 60% and runs for 10 minutes after the run command is removed.

For example, an ATV61HD18M3X drive (size 6), the heatsink fan starts when a Run command is given.

d
Here is a table indicating what drives are included for each Frame size:
s
NOTE that the frame sizes listed are the global engineering frame sizes.  Some documents from the US may have slightly different labels.

Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: