Do I need to change my PC ‘s TCP/IP parameters to discover the devices in the network?Yes. You need to change the parameters in your PC if the devices connected are not in same subnet mask. Please refer the installation guide.
Опубліковано для:Schneider Electric Україна