Video: How do I create Dynamic Messages in Vijeo Designer V6.2?
This video demonstrates how to create a dynamic event messages in Vijeo Designer V6.2.



1) Create a new Vijeo Designer application.

2) Create a new variable.

3) Create a new text resource.

4) You can add a variable to a message using this syntax
The tank level is: <var:TankLevel>

5) Create an Event group.

6) Add an Event Summary to a panel.

7) Add a numeric entry field for testing purposes.

8) Create a periodic action to trigger the event.

9) Use the Vijeo Designer simulator to test that application.

Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: