What is the part number for an Apogee P1 option card for the ATV630/ATV930 drive?
Issue:
Part number for the Apogee P1 option card for the Process drive

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
Attempting to add the ATV630 to a Apogee network.

Resolution:
There is currently not a Apogee P1 option for the ATV630 or ATV930 process drives.  Consider using a 3rd party's gateway to an embedded protocol.

Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: