VIDEO: Testing Citect Credentials Fail for Application Services Host
Issue
A users credentials fail to authenticate in Application Configuration Utility > Application Services Host:

Citect connection unavailable.
Note: Citect runtime must be running to perform this test

Note: Citect Runtime is already running.


Product Line
PowerSCADA Expert 8.1, 8.2, 9.0 (PSE 8.x, 9.x)

Environment
Application Configuration Utility

Cause
A successful connection by the Schneider Electric ApplicationServiceHost service requires a user already defined in the PowerSCADA project, server IP address and a parameter in the INI file.  However, testing citect credentials will not work if it's running as a service. In this resolution, the INI parameter is missing.


Resolution
1.  In Citect INI file, set [ctAPI] Remote = 1.




2.  Shutdown and restart the Runtime (project).

3.  Now the test will succeed:


**Embed video here**

Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: