Power Monitoring Expert 8.2 - When I run Report Generator (RepGen) from either an Engineering or Reporting Client, choosing 'Manage' causes a run-time error
Symptoms:
I launch Report Generator (the Excel-based reporting tool) on either an Engineering Client or a Reporting Client.
I choose the 'Manage Reports' radio button, and select any report.
At this point, an error dialog appears with the following text:

Run-time error 91:
Oject variable or With block variable not set


Workaound:
This will only happen if RepGen is run from either and Engineering or Reporting client and the version of Excel used is a newly installed x86 (32 bit) version of Excel 2013. The 64-bit version will work fine, as will the 32-bit versions of Excel 2007 and Excel 2016, as will using any  version of Excel and running RepGen on the server.

Schneider Electric Україна