How many finger-style vertical cable managers are required to fully populate one rail in a NetShelter cabinet?
Issue:
Customers need to know how many cable managers are required to fully populate one or more rails in a cabinet.

Product Line:
NetShelter, vertical cable management.

Environment:
All versions and serial ranges.

Cause:
It is unclear how many cable managers are needed to fully populate one rail.

Resolution:
For all of the following skus, quantity 1 contains two cable managers that will populate one (1) vertical rail height:
AR7580A
AR7585
AR7588
AR8442
AR7721
AR7722
AR7723

Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: