How do you set an ATV320 to run at a single speed?
Issue:
ATV320 to run at a single speed

Product Line:
ATV320

Environment:
All Serial numbers

Cause:
No External speed reference.

Resolution:
Enter and scroll down to CONF > FULL > SIM
Set LSP [Low speed]  to value desired as this will be considered your speed reference.
Motor frequency at minimum reference, can be set between 0 and [High speed] (HSP).

Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: