Initially ensure that all menus are uploaded, after connecting to the device with eSetup Easergy Pro select upload icon and “Read all settings”. Next select all signals used to “In use” under Communication/data maps. Then select tool icon and “Export ICD/SCL file…”. Before generation you need to define if RCB names should include indexes (typically selected) and if the file should be in Ed.1 or Ed.2 format. If Edition 2 extensions ae selected the file will have Ed.2 format, otherwise Ed.1 format. When saving the file there is the possibility to save the format as .icd, .iid or .cid.
Опубліковано для:Schneider Electric Україна