How many analog outputs AQ are standard on the ATV600 and ATV900 drives?
Issue:
How many analog outputs AQ are standard on the process drives?

Product Line:
ATV600 and ATV900 series

Environment:
All

Cause:
Analog outputs standard on the ATV600 and ATV900 drives.

Resolution:
There are two analog outputs standard on the ATV600 and ATV900 process drives, AQ1 and AQ2.

ATV600:

atv600 aq


ATV900:

atv900 aq

Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: