What is maximal cross section of the cable at front and rear terminals? Asfora, EPH57001xx loudspeaker outletsMaximal cross section for connection at front and rear terminals is 2,5 mm2. It is only suited for cables for loudspeakers.
Опубліковано для:Schneider Electric Україна