What is the default IP Address of the M580 PLC?Article available in these languages: Spanish
The default IP Address of the M580 is 10.10.x.x. The x.x is the last two octects of the MAC Address converted from Hexidecimal to Decimal.
Опубліковано для:Schneider Electric Україна