Can NetShelter horizontal cable managers be mounted back-to-back?

Issue:
A customer is asking if the horizontal cable managers can be mounted back-to-back.

Product Line:
NetShelter Horizontal Cable Managers

Environment:
AR8600A, AR8602A, AR8603A, AR8605, AR8606, AR8612

Cause:
In some installations it may be advantageous to mount the horizontal cable managers on both sides of the mounting rail.

Resolution:

Yes, the horizontal cable managers can be mounted back-to-back. Please see the installation sheet: http://www.apc.com/salestools/BFER-8KYNMU/BFER-8KYNMU_R2_EN.pdf

Schneider Electric Україна

Досліджуйте більше
Серія:
Досліджуйте більше
Серія: