Do the PowerLogic and ION meters support low voltage DC power supplies?
Issue
Customer would like to determine available DC Low Voltage Supply options for a meter

Product line
PowerLogic Meter
ION Meter

Environment
Power Supply

Cause
Customer wants to determine available DC Low Voltage Supply options for a meter

Resolution
MeterSpecification
ION9000No DC low voltage supply option
ION7550/7650 20-60 V DC
PM8000 series20-60 V DC ±10 %
ION8650/8600Auxiliary DC low voltage supply 80-160 V DC ±20 % only
ION620020-60 V DC
CM4000 seriesNo DC low voltage supply option
PM5000 seriesNo DC low voltage supply option
PM800No DC low voltage supply option
ION7400No DC low voltage supply option
ION770020-60 V DC

Schneider Electric Україна