How to trigger a sag/swell waveform capture by monitoring the status of an external contact closure through the digital input of a PM8000 meter
Product Line
PM8000

Environment
PME 8.x
PME 7.x.x
PME 9.0

Resolution
*Warning: Before proceeding make sure you understand the following when using Designer
How to trigger a sag/swell waveform capture by monitoring the status of an external contact closure through the digital input of a PM8000 meter

Step 1.
Open Designer from the PME Folder
How to trigger a sag/swell waveform capture by monitoring the status of an external contact closure through the digital input of a PM8000 meter

Step 2.
Select the PM8000
File>>Open>>PM8000
How to trigger a sag/swell waveform capture by monitoring the status of an external contact closure through the digital input of a PM8000 meter

Step 3.
Click on Advanced Setup: Frameworks
How to trigger a sag/swell waveform capture by monitoring the status of an external contact closure through the digital input of a PM8000 meter


Step 4:
Select Power Quality
How to trigger a sag/swell waveform capture by monitoring the status of an external contact closure through the digital input of a PM8000 meter

Step 5:
Select Sag/Swell detection
How to trigger a sag/swell waveform capture by monitoring the status of an external contact closure through the digital input of a PM8000 meter

Note: The image below can vary depending on the customizations done by the customer but the default modules for sag/swell detection on a PM8000 should have a pulse merger that is connected to Waveform Recorders.  This pulse merger module will have all the inputs filled so we need to combine one input to include multiple triggers.

How to trigger a sag/swell waveform capture by monitoring the status of an external contact closure through the digital input of a PM8000 meter

Step 6.
Unlink the output of Man Wfm Trig and create a new Pulse Merger Module
To Unlink simply right-click on the input of the the Wfm Tg Mg-Sg/SW shown below

How to trigger a sag/swell waveform capture by monitoring the status of an external contact closure through the digital input of a PM8000 meter

Step 7.
Use the ION Modules tool box on the right to create a new pulse merger.
How to trigger a sag/swell waveform capture by monitoring the status of an external contact closure through the digital input of a PM8000 meter

Step 8.
The new pulse merger will be placed in between the Man Wfm Trg and the Wfm Tg Mg-Sg/SW
How to trigger a sag/swell waveform capture by monitoring the status of an external contact closure through the digital input of a PM8000 meter

Step 9.
With the new Pulse Merger, you can take the Man Wfrm Trig and the digital Port S1 and combine them and now you can feed that to the input of Pulse Merge 32 without having to change anything else.  So, in other words, you would just be adding a Pulse Merge Module in between Man Wfrm Trig and Wfrm Tg Mg-Sg/Sw.
How to trigger a sag/swell waveform capture by monitoring the status of an external contact closure through the digital input of a PM8000 meter
As you can see in the image above Pulse Merge 32 takes in Man Wfrm Trig and Digital input S1 and merges them to output to Pulse In 6.  So now the waveform capture can be initiated when it detects a digital input trigger without affecting any other default triggers pertaining to this device

Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: