Which database and table are the ENM Diagnostics tab events saved in

Issue
Customer would like to know database and table are the ENM Diagnostics tab events saved in.

Product Line
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0

Environment
Event Notification Module 7.0
Event Notification Module 8.x

Resolution
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*

Events are stored in:
  • PLES_Logging database
  • dbo.Log table
The events can be observed by querying the dbo.Log table in PLES_Logging database:
  1. Right click on the dbo.Log table
  2. Select the option: 'Select Top 1000 Rows'
*Note: As of PME 2020, an updated ENM configuration was introduced. The Integrated Event Notification Module includes a new notification engine that seamlessly integrates with PME for alarm-based notification.*

Schneider Electric Україна

Досліджуйте більше
Серія:
Досліджуйте більше
Серія: