Пошук серед найпопулярніших питань
Как узнать, в какой версии Zelio Soft 2 было запрограммировано реле (какая версия ПО нужна, чтобы выгрузить программу)
Для этого необходимо зайти в меню - Version
В данном меню нас будет интересовать строка "Firmware" и следующая (см.фото)
Ниже указано, какая версия Zelio SoftII, с какими версиями firmware совместима:
*************************** Version 5.3 ************************
Firmware FBD V4.12 / V4.4.04
Firmware LADDER V4.11 / V4.3.01
Firmware LADDER EXTENDED V4.13 / V4.4.02
Firmware SR2COM01 V1.0.13
*************************** Version 5.2 ************************
Firmware FBD V4.12 / V4.4.04
Firmware LADDER V4.11 / V4.3.01
Firmware LADDER EXTENDED V4.13 / V4.4.02
Firmware SR2COM01 V1.0.13
*************************** Version 5.1 ************************
Firmware FBD V4.12 / V4.4.04
Firmware LADDER V4.11 / V4.3.01
Firmware LADDER EXTENDED V4.13 / V4.4.02
Firmware SR2COM01 V1.0.13
*************************** Version 5.0 ************************
Firmware FBD V4.07 / V4.3.01
Firmware LADDER V4.05 / V4.2.05
Firmware LADDER EXTENDED V4.09 / V4.4.03
Firmware SR2COM01 V1.0.13
*************************** Version 4.6 ************************
Firmware FBD V4.2.05
Firmware LADDER V4.2.05
Firmware SR2COM01 V1.0.13
*************************** Version 4.5 ************************
Firmware FBD V4.2.04
Firmware LADDER V4.2.04
Firmware SR2COM01 V1.0.13
******************************************** Version 4.4 ***********************************************
Firmware FBD V4.2.03
Firmware LADDER V4.2.03
Firmware SR2COM01 V1.0.13
*************************** Version 4.3 ************************
Firmware FBD v4.02
Firmware LADDER v4.02
Firmware SR2COM01 v1.0.12
*************************** Version 4.2 ************************
Firmware FBD v4.01
Firmware LADDER v4.01
Firmware SR2COM01 v1.0.12
*************************** Version 4.1 ************************
Firmware FBD v4.01
Firmware LADDER v4.01
Firmware SR2COM01 v1.0.12
*************************** Version 3.1 ************************
Firmware FBD v3.09
Firmware LADDER v3.09
Firmware SR2COM01 v1.0.12
*************************** Version 2.4 ************************
Firmware FBD v2.18
Firmware LADDER v2.19
*************************** Version 2.1 ************************
Firmware FBD v2.16
Firmware LADDER v2.16
*************************** Version 2.0 ************************
This version can be used to program automation applications
either by using LADDER diagrams as with Zelio Soft or by
using FBD (Functional Block Diagram) language.
Более подробно изменения, вносимые в ZelioSoftII описаны в файлах Readme:
C:\Program Files (x86)\Schneider Electric\Zelio Soft 2\Z2Readme