The wiring diagram in the manual only shows the 2-wire sensor connection of the module. Is there a wiring diagram for 3-wire sensor when using BMXDDI3202 and BMXDDI6402?
- Product Line
- Resolution
Comparing to the 2-wire sensor connection, customer need to add a Fuse in the single loop which the capacity should follow the off-status current in the sensor manual.
Опубліковано для:Schneider Electric Україна