This Knowledge helps the user to understand the limitations of service license with multiarea project.
When the customer has a multi-area project and he has activated the service license along with local Project addon service,then the addon works only for project with 1 area.It will let the customer to build the project on Builder with the “Unlimited local mode “option selected. But the project will expire after 15 days in the app.
The only workaround with multiarea project is to rebuild the project every 15 days.
This has been faced in AOA builder version 2.6.82.000 and AOA App version 2.6.1. But it is applicable for all the AOA versions.
Опубліковано для: Schneider Electric Україна