Solution:
- For Status Code error 3011, it corresponds to: "The object for storing status information about a 6000 series I/O module could not be found." Similarly, Status Code 3010 corresponds to a 5000 series I/O module error.
- The I/O Configuration page shows a Status Object for a module (PIO_SP474_Status in the image below), but the Object isn't appearing in the Object Configuration table.
- Go to Configuration > Physical I/O > Local and highlight the module with the affected missing Object.
- Select Clear Status Object
- Make sure the box is checked, then press Yes to conform, then Apply
- Replace the module's Status Object with the Add Status Object button and create an Object Association with a new object or an existing object.
- Apply the changes to the database.
- Verify that all of the Status Objects appearing in your I/O Configuration are appearing in the object database. Repeat Steps 1-5 for any additional modules that are missing their status objects in the database.
Опубліковано для: Schneider Electric Україна