Depending on the specific application, you may want to integrate a MC12 system into a larger machine model. To do this, you must first have the MC12 system generated by Machine Expert Twin. During generation, Machine Expert Twin creates a separate section for all MC12 related objects. Afterwards you can integrate the section and all MC12 objects in your model.
In order to be able to move the MC12 system in the model, you can simply select the section and change its position. This will move all MC12 objects together. Moving individual MC12 objects can cause problems and interrupt the track.
All other objects of the machine model should then be organized in separate sections.
Опубліковано для: Schneider Electric Україна