Пошук серед найпопулярніших питань
Using the BMENOR2200 with DNP3 Group 12 Variation 1 binary output TCC command.
In order to use the BMENOR2200 Ethernet module with Group 12 Variation 1 binary output Trip Close Command, the DNP3 point must be configured as shown:
The format for the DNP3 Group 12 Variation 1 'Trip Close Command' select range specifier and object prefix sent by the device must be according to the following example:
- Configure the Trip Close mode.
- Configure the binary output point TCC for Trip_Close.
The format for the DNP3 Group 12 Variation 1 'Trip Close Command' select range specifier and object prefix sent by the device must be according to the following example:
Опубліковано для:Schneider Electric Україна
Досліджуйте більше
Продукт:
Досліджуйте більше
Продукт: