Issue:
What is our policy on using an APC UPS inside a vehicle for portability and/or mobility?
Product Line:
- All Back-UPS models
- All Smart-UPS models
Environment:
All models of Back-UPS and Smart-UPS being used in a vehicle by using an inverter.
Cause:
Using a UPS in a car can expose it to high temperatures, vibrations, and potential shocks, which can damage the unit and shorten its lifespan.
Resolution:
Schneider Electric recommends against using your APC UPS in a car or any vehicle. For safety reasons, it must be plugged into a properly grounded electrical outlet. APC UPS units are intended for stationary indoor use and should be placed in a stable, well-ventilated environment. Additionally, we do not recommend using your APC Smart-UPS/Back-UPS as a portable power supply that is repeatedly discharged/recharged (like on a portable equipment cart). These units are designed to provide uninterruptible power for emergency use during unexpected power outages or momentary loss of power.
Опубліковано для: Schneider Electric Україна