Why can't I downgrade the BMENOC0321?
This is due to a new NAND Flash hardware component introduced in Product Version (PV) 26 and greater.

If you have a BMENOC0321 that is PV26 or greater, the lowest acceptable firmware level is v1.08.The downgrade procedure will fail if you attempt to downgrade the firmware below v1.08 with a PV26 or greater.

For more information on the BMENOC0321, please visit SE.com.

Schneider Electric Україна

Досліджуйте більше
Продукт:
Статті, які можуть бути корисними
Досліджуйте більше
Продукт: