Issue:
If required, a Remote Emergency Power Off (REPO) function can be connected to the Symmetra LX. It is a critical safety feature that allows for the immediate shutdown of power to the electrical equipment in emergency situations. When wiring a Symmetra LX UPS for REPO, it's essential to adhere to all safety guidelines and local electrical codes.
Product Line:
Symmetra LX
Environment:
All serial numbers
Cause:
The purpose of this document is to provide users with a wiring guide for implementing the REPO (Remote Emergency Power Off) feature on a Symmetra LX UPS.
Note: In many locations, the Remote Emergency Power Off (REPO) switch must be installed by a licensed electrician. Refer to local and national codes. See the Symmetra LX Safety and General Information Guide or the attached file for REPO requirements and detailed safety instructions.
Resolution: