{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the default password for the PM700 Power Meter range ?

To begin power meter setup, do the following:

1. Press ...>  until you see SETUP
2. Press SETUP
3. Enter your password.

The default password is 00000.

If this password has been changed please make sure you make a note of the new password as it cannot be reset

Please note the PM700 range is now obsolete, for information on replacement please see FAQ FA264122

Schneider Electric UK

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.