{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How is the ICMP Ping utility setup in ConneXview?
The ICMP ping control inside of ConneXview has 2 components, one component for discovery of network nodes and another that monitors the node.

See graphic below for the configuration feature that controls the ICMP ping feature.



For the Discovery of a node on the Ethernet network, The user can configure how long ConneXview will wait for a response during discovery before determining if a device is active at an IP address. This is set under the section "ICMP Communication". The default value is 1 second with 1 retry.

For the Monitoring of a discovered node on the Ethernet network, The value for the periodic ICMP ping is set under the section "Device IP Monitoring". If the device fails to respond to the periodic ICMP ping every 20 seconds by default, then an alarm is generated.




Please note that ConneXview is now a legacy product that is not longer commercialised

Schneider Electric UK

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.